6/26/2013 7:30 PM | |
Posts: 45 Rating: (0) |
HELLO, when i connect with a simocode of a damper, and i want to download the configuration, the GEN.FAULT come the FLASHING IN RED knowing that i have did athe good configuration you will find bellow what i'm did at the configuration, and what's happened when i'm with a simocode online(in the picture 3) by the way, when i change the application from valve1 toreversing starter(Picture 4), the GEN FAULT stopped. is that the solution? Attachmentpic.ZIP (238 Downloads) |
6/30/2013 6:37 PM | |
Posts: 45 Rating: (0) |
HELLO in the existing installation of the plant, it exist the same Consumer(equipement) as mine, it's a diverter gate so it's not the setting of paraméters I assure you my friends, and I used the GSD file of the existing take a look of my folder bellow is that can be the probléme of the Limits switch? at the wiring I found that are wired on the principle of Normally open, that can maybe done on Normally closed??? by the way ''VALLI'', when i chang the application from valve 1, to reversing starter, the GEN FAULTdisappeared. thanks for an answer as soon. AttachmentGSD+PIC.ZIP (221 Downloads) |
Last edited by: f.hamza at: 6/30/2013 7:19 PMLast edited by: f.hamza at: 6/30/2013 6:39 PM |
|
Follow us on