3/7/2019 2:23 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating:
|
Dear Experts, I'm Working on resolving one downloading issue to AS AS: 417-4 ES: PCS7 V8.0 OS: WinCC Redundant Server My issue is that Whenever I try to do Entire compilation with "Generate module drivers" its showing 17 Error counts. Kindly look at the attached image, It's showing some type of connection names in detail view, I couldn't figure out Such kind of connections or textual link etc using POV and Cross-reference throughout the project. Will any of you can tell that where I can look for such type of block connections mentioned in Module driver error log tab: ERROR: THE DESCRIPTION OF OBJECT "PN_NORM1_LINK1 WAS NOT FOUND IN FILE 08000000\AL_DPNDRM.XML\PN_NORM1_LINK1 And, The Program backup allowing to do changes only or entire compilation without generating module drivers But, Not allowed to do a download of "Changes only", "Entire download". it's Asking for "To test CPU" option otherwise (Start button shows) AttachmentCompilation_GMLDRVR_Error_3.zip (137 Downloads) |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
3/7/2019 6:42 PM | |
Joined: 2/1/2010 Last visit: 7/12/2024 Posts: 148 Rating:
|
Maruthakasi_S, If you open your HW config, does it give any messages about missing packages? (especially PDM) If so, you need to resolve this before compilation of any module drivers can be achieved. There are many other forums posts about resolving that issue. If not, probably more information is needed. |
If my post helped you, please rate. Thanks. |
|
3/9/2019 10:07 AM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating:
|
Hello Experts, I have Figured out the Error, And, described below. But, I couldn't give solutions to it. I will be happy if somebody can suggest the possible solutions, This Error is Present on both case either Entire compilation or changes only to Generate module drivers selection. And, It's not occurring for both case, if I didn't choose "Generate module driver". I noticed the Issue, We have connected 17 Nos of Siemens PAC3200 Energy meters 17 on Profibus network. This Profibus network created using IE/PB Link which is connected on CP 443-01.I have mentioned the MLFB details below, If I remove the PAC3200 slaves from the Profibus network the Error count getting reduced. And, When I removed entire Profinet I/O link (IE/PB converter, PAC3200 Slaves) there were no errors. And, I could do both categories of Compilations with Generate module driver selection. So, I wonder how this IE/PA link network creating such issues. And, I'm looking forward to the possible support from you all, Hardware family Details: PCS7 Version: PCS7 V8.0 CPU: 417-4 : 6ES7 417-4XT05-0AB0 PAC2300 Energy Meter: 7KM9 300-0AB00-0AA0 PAC3200 GSD File: S1018163 IE/PB LINK PN IO: 6GK1 411-5AB00 - V2.1
AttachmentCompilation_Error_Img.zip (103 Downloads) |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
3/9/2019 3:27 PM | |
Joined: 2/1/2010 Last visit: 7/12/2024 Posts: 148 Rating:
|
Is this your original engineering station or a newly installed one? I think it must not the be original es for the project. I think you are missing packages/libraries that were originally present such as sentron pac library and as- interface library. Check your blocks folder for blocks from sentron author or something similar. I can't recall the correct author name. Based on looking at your original compile log I can see you have as-i master installed. As-i will somewhat work ok but no diagnostics without library, but sentron pac you will need to change method of integration. Probably change or delete charts with those blocks from the sentron library and replace the code with your own function, or obtain and install the library to your es. I recall having a similar problem with XML files when facing a pac controller that was integrated without the library in a past project. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
3/11/2019 6:26 PM | |
Joined: 2/1/2010 Last visit: 7/12/2024 Posts: 148 Rating:
|
I don't think anyone can/should provide the Sentron PAC library on this forum as it is protected by paper COL license only. You'd better contact your sales rep, or use iMall. https://support.industry.siemens.com/cs/document/109744690/ https://mall.industry.siemens.com/mall/en/us/Catalog/Products/10048962 |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
Follow us on