3/7/2018 11:29 AM | |
Joined: 5/23/2017 Last visit: 11/19/2018 Posts: 10 Rating:
|
Hello guys, //Can I please move this topic to section Communication / Networks ? Something went wrong with categories during writting this topic :/ // I am expecting a problem with warning like written in topic when going online with my PLC: "Going online: the HW configuration of the HMI_RT_1 was changed but it was not compiled and loaded yet. The shown diagnostics is possibly inconsistent or wrong." The problem was found when HMI started to say: "No diagnostics data available because the current online configuration differs from the offline configuration data." in device view. I want to solve it and make it work without warnings but internet knowledge about this problem didn't help me yet. I tried to compile entire HW, SW, download all again but the problem still exist and can't figure what could be wrong. Devices are working in topology as shown in the additional attachement. I would be grateful for help to solve this. If any additional informations are needed please let me know, I will do my best. I have also attached an image with problematic errors shown. - Operating System: Windows 10 PRO 64x, compilation number 16299 - TIA Version : V14 - Hardware Modules numbers : CPU: CPU 1513-1 PN, 6ES7 513-1AL01-0AB0, FV v. 2.1 HMI's: 2 x TP700 Comfort, 6AV2 124-0GC01-0AX0, FW v. 13.0.1.0 |
Last edited by: Nutaharion at: 3/7/2018 11:34:37 AM |
|
3/7/2018 11:30 AM | |
Joined: 5/23/2017 Last visit: 11/19/2018 Posts: 10 Rating:
|
Topology attachment |
Follow us on