10/13/2008 5:31 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating:
|
Hi, which STEP7 version and Windows do you have? |
Denilson Pegaia |
|
10/13/2008 7:05 PM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating:
|
Windows XP Professional SP3 and Step 7 V5.4 SP4. |
10/13/2008 7:33 PM | |
Posts: 487 Rating:
|
Windows XP SP3 is not supported by Step 7. Please see the link for SP3 uninstall procedure http://support.microsoft.com/kb/950249 |
10/14/2008 8:44 AM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating:
|
Sorry JMJ but is not good idea because rest of hardware updates was installed without problem. |
10/14/2008 4:54 PM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating:
|
Sorry JMJ attached you found README.pdf file and chapter 3 : 3.1 Operating Environment Operating systems STEP 7 V5.4 including SP4 is a 32-bit application whose functionality has bee approved and released for the following operating systems: • MS Windows XP Professional SP3 • MS Windows Server 2003 SP2 Standard Edition with or without R2 as workstation computer • MS Windows Vista 32 Bit Ultimate and Business with / without SP1 Bye. AttachmentREADME.pdf (322 Downloads) |
10/14/2008 11:28 PM | |
Posts: 487 Rating:
|
Now, I see what you are saying. Sorry to bring up SP3 issue. But check the SP4 release notes http://support.automation.siemens.com/WW/view/en/29753194 It says compatible with XP SP2 and PDF says SP3. You want to clarify this with tech support. |
Follow us on