7/5/2010 9:51 PM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating:
|
Hello faming,
Failed?! Do you mean internally? like losing the optocoupler?! Unfortunately you can't have it. The only S7-300 digital input module that supports diagnostics is the 7BH01 module. However, the channel diagnostics that you can get from this module are: 1- Wire break (ashunt resistormust be connected to transducer contacts). 2- Missing supply voltage. The other diagnostics refer to the module itself not to channels (Check attachment). Best regards. H-H Attachment7BH01.pdf (109 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on