7/29/2014 7:55 PM | |
Posts: 56 Rating: (1) |
It seem that the CP443-1EX30-0XE0 is not able to be set up as a Profinet Controller...Can someone please verify? Thanks again! |
7/29/2014 8:50 PM | |
Posts: 56 Rating: (1) |
I see that it say that in the manual. But when I go to set it up in my hardware config there is no checkbox for profinet IO controller. There is however this check box on the CP443-1EX40. But then I run into another issue saying that my profinet Node is not compatible due to something to do with diagnostics. |
7/29/2014 9:40 PM | |
Posts: 56 Rating: (1) |
Ok I have an answer for others in the future. I had to right click on Insert Profinet node...not double click on the module. The IM151-3 works fine with this CP. |
This contribution was helpful to2 thankful Users |
Follow us on