5/31/2021 9:24 AM | |
Joined: 1/3/2013 Last visit: 6/18/2024 Posts: 40 Rating: (3) |
Dear friends, I just received my SIMATIC ET 200SP Open Controller, 6ES7677-2SB42-0GL0 which has a CPU 1515SP PC2 F + HMI 512PT, 8 GB RAM, 128 GB CFast with Windows 10 IoT Enterprise 64-bit, S7-1500 Failsafe Software Controller CPU 1505SP F and WinCC Runtime Advanced pre-installed. Since I don't have experience with open controllers, I considered studying the Getting Started Open Controller video series (which is a very nice approach). I followed the steps presented in the getting started material, and created my hardware configuration and a small WinCC application in TIA Portal V16. Everything compiled without errors and I decided to load my configuration. I connected my hardware on X2 ethernet port and triggered the loading process of the hardware & software. TIA portal managed to find and connect to the PC System, transfer its configuration and application of the WinCC ..... but could not find the Software PLC. The overall download process was not completed. I went online to check for more info in diagnostics and find that my Software Controller is powered off or missing. (I attached an picture). My question is how to start the software controller? since I'm sure that it is already installed. Best regards, Mircea. |
Follow us on