8/2/2016 7:42 PM | |
Joined: 12/7/2011 Last visit: 8/11/2024 Posts: 384 Rating: (9) |
Hi to all. Many times i thinked how could be possible save my old CP5512, and use it with my new laptop. After much time spent on the net, i've read many post about it, and few days ago, i've bought an "ExpressCard/34 to CardBus" adapter for perform the tests by myself. So the result of the test has been great . The CP5512, work properly with all the functions, Software, HW, Diagnostic, PDM and so on. During my tests the only strange things i saw, has been when in the setting PG-PC interface, i've tryed to test the CP. In this case the test has failed, but to be honest i think i know (i'm not totaly sure) the reason, in the specifications of the adapter is highlighted that the adapter does not support the 32 CardBus +5V. In this case i think that some problem could come out if you need to provide to power at the loop. But beyond that, the most importants features are been tested. For me is a gol, and hope this Tip will help someone. Regards. Duccio. PS: If this post did really help you, you may use the Rate-button AttachmentCP5512.pdf (407 Downloads) |
Last edited by: Duccio at: 8/2/2016 7:45:01 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on