2/10/2010 9:18 PM | |
Posts: 2 Rating: (0) |
Hello, First of all, this is the configuration: PS3072A CPU 315-2 PN/DP (eh13) CP 343-1 Advanced (gx21) 4x SM331 (1kf01) SM321 (1bL00) SM332 (5hf00) SM322 (1bh01) The problem is the following: After I set up the MPI-PC network, I make the correct hardware configuration in S7, set an IP address to the PLC CPU's port (the CP module not networked) and download it to the module (not the whole station just only the hw config). After that, when I start (run) the PLC the SF LED becomes red it goes to STOP mode. (DC5V is green) I can't do again the hardware downloading step, because I get this error message: "The system data cannot be loaded to module!" (13:4589) I can download again if I reset the CPU's memory. There are some strange things: I see the CPU-PC network with "Display accessible nodes" and can run "Hardware diagnostic" and "Module information" from the menu. I can't receive replying message after pinging ethernet port from prompt the. I can't download the whole station to the PLC. I can't download update the hw config unless I reset the memory again. (I checked third that the correct module is in use in the hw config. If I try to use "Open online" function form the hw config menu, the online config's cpu and cp are displayed in gray OR get this message :"Cannot establish the connection..." I stopped and disconnected the CP's ethernet port because I use the CPU's port. What works: -I see the PLC's CPU via MPI after "Download to module" step. -I can download the hw config to the module at once. (SF is on) I would like to set and download the correct hw config to the module because I think, this is the problem. I attached some pictures about the errors. Please help me to find the solution! Thanks. Attachmenthibák.zip (191 Downloads) |
2/10/2010 11:57 PM | |
Joined: 10/7/2005 Last visit: 7/15/2024 Posts: 3009 Rating: (1053)
|
Hello libertitas Imust admit it seems like a strange problem and one that Inot have had yet. While theStep 7error code list (which you can download HERE) does list error "13:4589", it is relatedto the configuration ofH connections(which you wouldn't be able to use or needin a 300). Your screendumps do unfortunatelynot contain the a picture of the "Details" window so its hard to say if this suggested remedy is applicable or not. I suggest you try it anyway (delete the SDB system data folder from your Blocks folder and recreate it by compiling HWconfig AND NetPro) and let us know if it helped. If it doesn't, please post the contents of the "Details" window (there is a "details" button on theerror popup window that you get when your download fails). Ihope this helps |
Cheers |
|
9/15/2014 4:16 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by Johannes4uis split to a separate thread with the subject hardware Config download problem. Best regards Min_Moderator |
Follow us on