7/26/2023 10:00 AM | |
Joined: 5/6/2022 Last visit: 7/5/2024 Posts: 429 Rating: (83) |
Hi naorasse, One question, is the project you have a PCS 7 type? I am telling you this because it is likely that the project is of the PCS 7 type and that is the reason why the option appears disabled. In Simatic Manager, you must go to the project properties and in project type STEP 7 must be selected. Could this be the reason? Best regards!
|
If this Information really helps, you could use the Rate function |
|
7/26/2023 12:02 PM | |
Joined: 12/19/2021 Last visit: 7/12/2024 Posts: 5 Rating: (0) |
thank you very much, you are right I have now selected type step 7 in property of project |
Follow us on