12/16/2013 1:42 PM | |
Posts: 26 Rating: (6) |
Hi,JohnJohnJohn. This management has to help on KNX.I recommend to study application .vd for KNX Tool (ETS).
AttachmentGesamtdoku EIB A4e.pdf (374 Downloads) |
1/3/2014 9:46 AM | |
Posts: 215 Rating: (6) |
Hi JohnJohnJohn, please look up the manual please refer to manual http://support.automation.siemens.com/WW/view/en/50074616 At page16 you will find information about the amount of ins and outs also via ethernet. "Each LOGO! Base Module supports the following connections for the creation of the circuit program, regardless of the number of connected modules: ● Digital inputs I1 to I24 ● Analog inputs AI1 to AI8 ● Digital outputs Q1 to Q16 ● Analog outputs AQ1 to AQ2 ● Network digital inputs: NI1 to NI64 ● Network analog inputs: NAI1 to NAI32 ● Network digital outputs: NQ1 to NQ64 ● Network analog outputs: NAQ1 to NAQ16" You can run up to 8 LOGO! basic modules on one net (SIMATIC S7 communication)with one central program or different decentral programs. The specification regarding CM EIB/KNX is to be found on page 342. Regards |
Follow us on