7/25/2017 12:33 PM | |
Posts: 75 Rating: (0) |
Hello experts, It's first time that I connect 2 plcs by profibus (2 s7300 plcs with cpu315F 2 pn/dp). Diagnostic buffer of module CPU 315F-2 PN/DP Please help me. Thank you a lot. Best regards. ------------------------------------------------------------------------------------------ AttachmentDiagnostic buffer of module CPU 315F.txt (188 Downloads) |
Last edited by: Jen_Moderator at: 7/26/2017 1:37:45 PMNew subject after splitting Last edited by: Jen_Moderator at: 7/26/2017 1:41:19 PMAdded Diagnostic Buffer as an Attachment. |
|
7/25/2017 1:37 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, Parameter assignment-error means that you have errors in the HW-Konfig. have a look to this entry: What master/slave communication options are available on PROFIBUS DP? I´m pretty sure you find a right application sample that shows you the right way to configure your master-slave-configuration. hope this helps, regards, |
FCK WAR! |
|
7/25/2017 3:13 PM | |
Posts: 75 Rating: (0) |
Thank you very much for fast answer. I'm confused because my plc has CP-343 module (AS Interface) and I can't find any example with that communication processor. I can't find profibus properties like in this samples you send me:
|
7/25/2017 3:42 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, AS-I is not Profibus. If you don´t have a Profibus-CP to communicate over Profibus, I think this application sample/FAQ may be the best : DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3hope this helps, regards, |
FCK WAR! |
|
7/26/2017 2:49 PM | |
Posts: 75 Rating: (0) |
Thanx Jen. Event 8 of 10: Event ID 16# 5961 Parameter assignment error in CPU module parameters Parameter: module type Output address: 384 of the module with parameter assignment errors Error type: type ID not detected ID Operating mode: STARTUP (warm restart) External error, Incoming event 10:30:42.479 PM 01/19/1994 (Coding: 16# 5961 FF06 C17B 0001 0180 8B07)
How to set configuration in DP slave properties? Which adresses, unity, lenghts, consistency? |
7/26/2017 2:56 PM | |
Posts: 75 Rating: (0) |
Event 8 of 10: Event ID 16# 5961 Parameter assignment error in CPU module parameters Parameter: module type Output address: 384 of the module with parameter assignment errors Error type: type ID not detected ID Operating mode: STARTUP (warm restart) External error, Incoming event 10:30:42.479 PM 01/19/1994 (Coding: 16# 5961 FF06 C17B 0001 0180 8B07)
Do you have some instructions how to set DP slave propperties, how to set adresses, lenghts, unities and consistency? |
7/27/2017 1:00 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice.
|
Follow us on