2/17/2011 3:36 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi neoser, Sorry, your problem not open to me?? Can you tell little more, But, maybe you can use this tool to monitor your Micromaster. http://support.automation.siemens.com/WW/view/en/11769381 Best regards, -Heksu- |
"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
2/18/2011 12:57 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi, First front panels rs connection 6SE6400-1PC00-0AA0 text from: http://support.automation.siemens.com/WW/view/en/26437233 " 1 This is also valid for all other operator panels. You can find information on this in Catalog Operator Panel OP 6SE6400-0SP00-0AA0 2 As an alternative, to establish a connection to the PC, an RS485 – RS232 converter can also be Attachmentmm420gettingstartedguide.pdf (181 Downloads) |
"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
2/18/2011 1:11 PM | |
Posts: 6 Rating: (0) |
Hi Heksu yes, you have an accurate estimate. I haven't rs232 connection point. I have RS232 cable and rs232 converter to usb, so I generally use usb, but you said that RS485 and RS232 are not scome of supply of the converter. I want to use without kit. is that possible? |
2/18/2011 7:57 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
You mentioned in your first post that you are using 7-9 DI i.e. DI-3 for speed boost so P703 will be 3 and you are using 6-9 DI i.e. DI-2 for speed reduce then P702 will be 14... Now regarding your problem to be online.. You cant use your RS 232 direct as MM430 doesnt have any RS232 connection. It has RS 485 on terminals 29-30 so if you dont wanna buy PC kit, then you must use RS 485-232 converter. Without this, you will not be able to connect your drive to PC... From BOP, it is not too hard.. Just try Quick commissioning as said in Operatig Instruction and Set control Paramters as I suggested and I guess it should work easily... Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
2/21/2011 10:15 AM | |
Posts: 6 Rating: (0) |
Thank you for everything Now I understood that the location is not important, what I want to use, it is our choice 13-14 or 14-13 I looked the operating instructions and I saw 29-30. I have rs485 cable too. I send you it's picture, but I didn't understand which pin is P+, which pin is N-. the operating instructions show that P+ is 29 and N- is 30 but which correspond on RS485 cable terminals. I send you RS485 cables's picture |
Last edited by: neoser at: 2/21/2011 10:23 AM |
|
Follow us on