9/29/2008 9:32 AM | |
Posts: 8 Rating:
|
Thanks, Dec! Where can I see Alarm table "MSMsgs"? I addeda picture which I hopecan clear up theissue.The main question is how does this construction in WinCC messages work? @1W%t#ErrTextLib@ |
Last edited by: Stalker at: 9/29/2008 9:51 AM |
|
10/3/2008 4:42 PM | |
Joined: 5/19/2006 Last visit: 6/20/2024 Posts: 548 Rating:
|
Hi, See the attached example STEP7 & WinCC integrated. Change the computer name in WinCC with your computer name and make sure you have defined CP_H1_1: access pointin Set PC/PG Interface. In HWConfig change CPU/CP (MAC, IP for your hardware). Compile OS. You will havemaybe awarning with group display hierarchy but it's normalbecause OS iscreated without OS-ProjectEditor (plain basic WinCC project). Ignore any STEP7 warnings of missing packages (PDM-Siprom etc) if you don't have those installed. You can use PLCSim for test. The following SQL tables are involved in formating the alarm message textin RT: CC_Step7Text, MsMsgs and WinCC Text Library table. Have fun Dec AttachmentTextLibExample.zip (476 Downloads) |
Follow us on