7/12/2007 7:38 PM | |
Posts: 6 Rating: (0) |
You need to download the Micromaster Profibus Optional Board Operating Instructions. Here's the link: https://support.automation.siemens.com/WW/llisapi.dll?filteron=on&csquery0=profibus+optional+board&aktprim=0&extranet=standard&func=cslib.csinfo&lang=en&nodeid0=10804922&objaction=csbrowse&objid=10804922&siteid=cseus&subtype=133300 Here is the number:6SE6400-5AK00-0PB0. I would have uploaded it but it was too large. Read this manual, play with it a bit, then you can ask some specific questions. This won't make sense now, but when you install the drive in Hardware Config, it will default toPP03 which will only allow you to send and receive control and status words. Since you want to read and write Parameters, you need to set it up with PP01 or PP02. |
Last edited by: tony moody at: 12.07.2007 19:42 |
|
7/16/2007 1:14 PM | |
Joined: 8/31/2005 Last visit: 6/14/2024 Posts: 2198 Rating: (328) |
Here you find some informations: http://support.automation.siemens.com/WW/view/en/22813212 |
|
|
Follow us on