2/1/2022 5:08 PM | |
Joined: 1/17/2006 Last visit: 7/4/2024 Posts: 553 Rating: (29) |
Hello ! 1. In the selection of the motor encoder in the Sizer, for example, "AM24DQI - absolute encoder 24-bit + 12-bit multiturn", it means that if I adjust fine resolution p418=2 (2-bit) I will have 6 -bit for multiturn: 32 (maximum) - 24 - 2 = 6-bit for multiturn ? 2. And does 6-bit for multiturn mean that a maximum of 64 turns can be evaluated by the encoder? 3. So, the total resolution will be 26-bit (24-bit + 2-bit) = 67108864 ? Regards, Berg
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/02/2022 08:43:01New subject after splitting "Educate the children and it won't be necessary to punish the men." |
|
This contribution was helpful to1 thankful Users |
Follow us on