8/9/2014 4:56 AM | |
Posts: 55 Rating: (0) |
Hi experts We got a problem with communication between CU240 with Sinamic S120 The system has: _PC with ethernet port _Switch _CU240 6AU1240-1AA00-0AA0 _Sinamic S120 6SL3040-1MA00-0AA0 Profinet address: C240: 192.168.10.55 S120: 192.168.10.56 Profibus address: C240: 2 S120: 4 The current setup is: the pc connect to c240 through ethernet and the c240 connect to s120 through profibus. the pc also have ethernet cable connect to the s120 through x127 port. We can see the C240 fine but can not recognise the s120 Can some one please help. Pics are attached Attachmentpics to ask.zip (176 Downloads) |
8/9/2014 8:46 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008)
|
Hi, ok you need the Sinamics SSP V4.6 for this Version of S120. The SSP you can download here. The SSP in included in STARTER V4.3.2.x but not in SCOUT 4.3.1.x ! Regards Christoph |
8/11/2014 11:01 AM | |
Posts: 55 Rating: (0) |
Hi, After i install the software I can see the the s120 through ethernet but not through profibus (as you can see in the picture) Really weird Can you pleasr help |
8/11/2014 11:09 AM | |
Posts: 55 Rating: (0) |
same with using Scout |
Follow us on