8/13/2014 3:31 AM | |
Posts: 55 Rating: (0) |
Yes, after change the address in DIP, I turn off the power and on again. Attached is the archived simotion scout project Can you please have a look P/S: can you please help send me your project layout if possible? AttachmentProjectSupport.zip (159 Downloads) |
Last edited by: tthoang86 at: 8/13/2014 3:34 AM |
|
8/13/2014 6:45 AM | |
Joined: 5/12/2006 Last visit: 10/17/2024 Posts: 22420 Rating: (3020)
|
Hi, ok now i see the problem. In your project no routing information is available for the route to the CU320 via ETHERNET. I have modify your project to this. Create a ethernet Subnet to the C240 Ethernet IF put a PG/PC in netpro to the project an connect it with the Ethernet assign the connectec PG/PC Interface in the PG/PC Object with the Ethernet Regards Christoph AttachmentD:\Testconf.zip (156 Downloads) |
8/13/2014 8:05 AM | |
Posts: 55 Rating: (0) |
Hic.. You are correct. That a silly mistake :( Thanks so much. It is working now |
This contribution was helpful to1 thankful Users |
8/13/2014 8:38 AM | |
Posts: 55 Rating: (0) |
Hi Chris Can I ask you another question? As we use the c240 to control the Cu320 through profibus. There are 2 servo motors, 3 and 4. We need to create AXES_Servo 03 and AXES_Servo 04. Thus need to use "Message Frame Type" for "Drive Asignment AXES" We tried to use the "standard Telegram 3, PZD-5/9" but it would not let us The picture and project is attached And please advice me which Telegram suitable or need enable any thing on CU320 Unit? Thank you very much AttachmentTest20140813_pics.zip (152 Downloads) |
Last edited by: tthoang86 at: 8/13/2014 8:43 AM |
|
8/13/2014 11:02 AM | |
Posts: 55 Rating: (0) |
Hi Chris There is still error. Can you please have a look and let me know what has been done wrong? and help me to correct it? Thank you very much, Chris. You are great help. Hoang AttachmentTelegramConfig_pics.zip (161 Downloads) |
8/13/2014 11:28 AM | |
Joined: 5/12/2006 Last visit: 10/17/2024 Posts: 22420 Rating: (3020)
|
Hi, i have corrected the project. The CU i have moved done toe the end of the list. Each DO with da PZD lenght 0 musst on the END of the list. An in the HWConfig a internal data was blocked the access, i have fixed this. Regards Christoph AttachmentD:\Telegr.zip (157 Downloads) |
8/13/2014 3:30 PM | |
Posts: 55 Rating: (0) |
Thank you Chris I will try it a let you know tommorrow
|
8/14/2014 6:04 AM | |
Posts: 55 Rating: (0) |
Hi Chris, Much appriciated your support. Thank make correct fault from you. May i have some question? 1. Please show me how to you did "An in the HWConfig a internal data was blocked the access" 2. After did HW config Telegram ok. I did MCC chart for test Axis_03 control Servo_03. But after downloaded to HW. C240 can not run and have alarm as attached file. pLease advice me the truble shoot. This first project i do SIMOTION. it is very complex. I Expect your support, Expert Chris!
AttachmentSIMOTION.zip (133 Downloads) |
Follow us on