4/1/2014 3:18 PM | |
Joined: 1/17/2007 Last visit: 7/5/2024 Posts: 1543 Rating:
|
A faster and better way is to use a lookup table. As there are only 256 possible values for each data byte, the CRC value for each data byte value can be precalculated and stored in a table. So you then just repeat for all bytes picking the correct value out of the table for each loop. Below is the code which I have tested and verified using an online CRC calculator. You set the CRCSTART value to the first data byte and CRCEND to the last data byte in the data storage area (DB?) that you are using. [code] FUNCTION_BLOCK CRC_CALC_8408 TITLE = 'CRC_CALC' AUTHOR : Smiffy VAR_INPUT CRCSTART : ANY; CRCEND : ANY; END_VAR VAR_OUTPUT CRC : WORD; END_VAR VAR CRCTable1 : ARRAY [0..127] OF WORD := 16#0000,16#1021,16#2042,16#3063,16#4084,16#50a5,16#60c6,16#70e7, 16#8108,16#9129,16#a14a,16#b16b,16#c18c,16#d1ad,16#e1ce,16#f1ef, 16#1231,16#0210,16#3273,16#2252,16#52b5,16#4294,16#72f7,16#62d6, 16#9339,16#8318,16#b37b,16#a35a,16#d3bd,16#c39c,16#f3ff,16#e3de, 16#2462,16#3443,16#0420,16#1401,16#64e6,16#74c7,16#44a4,16#5485, 16#a56a,16#b54b,16#8528,16#9509,16#e5ee,16#f5cf,16#c5ac,16#d58d, 16#3653,16#2672,16#1611,16#0630,16#76d7,16#66f6,16#5695,16#46b4, 16#b75b,16#a77a,16#9719,16#8738,16#f7df,16#e7fe,16#d79d,16#c7bc, 16#48c4,16#58e5,16#6886,16#78a7,16#0840,16#1861,16#2802,16#3823, 16#c9cc,16#d9ed,16#e98e,16#f9af,16#8948,16#9969,16#a90a,16#b92b, 16#5af5,16#4ad4,16#7ab7,16#6a96,16#1a71,16#0a50,16#3a33,16#2a12, 16#dbfd,16#cbdc,16#fbbf,16#eb9e,16#9b79,16#8b58,16#bb3b,16#ab1a, 16#6ca6,16#7c87,16#4ce4,16#5cc5,16#2c22,16#3c03,16#0c60,16#1c41, 16#edae,16#fd8f,16#cdec,16#ddcd,16#ad2a,16#bd0b,16#8d68,16#9d49, 16#7e97,16#6eb6,16#5ed5,16#4ef4,16#3e13,16#2e32,16#1e51,16#0e70, 16#ff9f,16#efbe,16#dfdd,16#cffc,16#bf1b,16#af3a,16#9f59,16#8f78; CRCTable2 : ARRAY [0..127] OF WORD := 16#9188,16#81a9,16#b1ca,16#a1eb,16#d10c,16#c12d,16#f14e,16#e16f, 16#1080,16#00a1,16#30c2,16#20e3,16#5004,16#4025,16#7046,16#6067, 16#83b9,16#9398,16#a3fb,16#b3da,16#c33d,16#d31c,16#e37f,16#f35e, 16#02b1,16#1290,16#22f3,16#32d2,16#4235,16#5214,16#6277,16#7256, 16#b5ea,16#a5cb,16#95a8,16#8589,16#f56e,16#e54f,16#d52c,16#c50d, 16#34e2,16#24c3,16#14a0,16#0481,16#7466,16#6447,16#5424,16#4405, 16#a7db,16#b7fa,16#8799,16#97b8,16#e75f,16#f77e,16#c71d,16#d73c, 16#26d3,16#36f2,16#0691,16#16b0,16#6657,16#7676,16#4615,16#5634, 16#d94c,16#c96d,16#f90e,16#e92f,16#99c8,16#89e9,16#b98a,16#a9ab, 16#5844,16#4865,16#7806,16#6827,16#18c0,16#08e1,16#3882,16#28a3, 16#cb7d,16#db5c,16#eb3f,16#fb1e,16#8bf9,16#9bd8,16#abbb,16#bb9a, 16#4a75,16#5a54,16#6a37,16#7a16,16#0af1,16#1ad0,16#2ab3,16#3a92, 16#fd2e,16#ed0f,16#dd6c,16#cd4d,16#bdaa,16#ad8b,16#9de8,16#8dc9, 16#7c26,16#6c07,16#5c64,16#4c45,16#3ca2,16#2c83,16#1ce0,16#0cc1, 16#ef1f,16#ff3e,16#cf5d,16#df7c,16#af9b,16#bfba,16#8fd9,16#9ff8, 16#6e17,16#7e36,16#4e55,16#5e74,16#2e93,16#3eb2,16#0ed1,16#1ef0; EndAddr : DWORD; END_VAR VAR_TEMP pDB : ANY; // Pointer for DB data DBAny AT pDB : STRUCT S7Code : BYTE; // Code for S7 = 16#10 DataType : BYTE; // Code for data type = 16#02 = byte Length : INT; // Repetition factor = Send/receive length DBNumber : INT; // Data block Number MemoryArea : BYTE; // Specified memory area = 16#84 = data block ByteAddressMSB : BYTE; // Byte address most significant bits ByteAddressLSB : WORD; // Byte address least significant bits END_STRUCT; u1Addr : DWORD; // Union pointer for calculation of byte offset address u1 AT u1Addr: STRUCT // This is equivalent to a union in 'c'. A dword goes in and word / byte LSB / byte MSB come out ByteAddrLSBPad : BYTE; // Not Used ByteAddrMSB : BYTE; // Byte address most significant bits WordAddr : WORD; // Byte address least significant bits END_STRUCT; CRCData : BYTE; CRCIndex : INT; CRCTemp : WORD; RetVal : INT; END_VAR pDB := CRCEND; DBAny.DataType := B#16#02; u1.ByteAddrLSBPad := 0; u1.ByteAddrMSB := DBAny.ByteAddressMSB; u1.WordAddr := DBAny.ByteAddressLSB; EndAddr := u1addr; pDB := CRCSTART; DBAny.DataType := B#16#02; u1.ByteAddrLSBPad := 0; u1.ByteAddrMSB := DBAny.ByteAddressMSB; u1.WordAddr := DBAny.ByteAddressLSB; CRCTemp := 0; WHILE (DWORD_TO_DINT(u1addr) <= DWORD_TO_DINT(EndAddr)) DO DBAny.ByteAddressMSB := u1.ByteAddrMSB; DBAny.ByteAddressLSB := u1.WordAddr; RetVal := BLKMOV(SRCBLK := pDB, DSTBLK := CRCData); CRCData := CRCData; CRCIndex := WORD_TO_INT(SHR(IN := CRCTemp, N := 8) XOR CRCData); // Calulate the lookup table index IF CRCIndex <= 127 THEN CRCTemp := SHL(IN := CRCTemp, N := 8) XOR CRCTable1[CRCIndex]; // Get actual CRC MSB from lookup table ELSE CRCTemp := SHL(IN := CRCTemp, N := 8) XOR CRCTable2[CRCIndex - 128]; // Get actual CRC MSB from lookup table END_IF; u1addr := DINT_TO_DWORD(DWORD_TO_DINT(u1addr) + 8); END_WHILE; CRC := CRCTemp; END_FUNCTION_BLOCK [/code] |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
This contribution was helpful to
2 thankful Users |
11/27/2019 4:55 PM | |
Posts: 1 Rating:
|
Hi Smiffy, I am trying to implement this code in a Function Block, using TIA Portal version V15.1 Update 3. Do you have the source code for this version?
|
Follow us on