3/15/2015 4:31 PM | |
Posts: 9 Rating:
|
I have a CPU 313c-2dp and CP5611. I have installed CP card in PC and its working properly. Currently my PLC and PC station is connected through profibus cable. First : do i need to make OFF on both sides (plc and pc station) on profibus connector or plc side off and pc station on or vice versa? Second : I need to acess memory words from my PLC through OPC. MPI port is connected to HMI . i wish to make s7 connection over profibus between the CPU 313 c-2dp and PC station (CP5611). I have got a document "Guideline_S7_PB_e.pdf" which shows how to make the s7 connection in PC station to a unspecified partner. In this my doubt is who is master and who is slave ? what should be config of the s7 station and PC station so that i can access the memory words in opc? Also in the attached file there is a document which shows how to make CPU as master and pc station as slave and my HW config snapshot. I am stuck after that point. Please help !!!!!!! Attachmentdpslaveconfig.zip (66 Downloads) |
3/15/2015 5:15 PM | |
Posts: 9 Rating:
|
i have a simatic net v12 |
3/15/2015 5:46 PM | |
Posts: 9 Rating:
|
here is another document i found which allows s7 connection over profibus. In this i have doubt: between cpu and pc station which is master and which is slave? link: http://support.automation.siemens.com/WW/view/en/15364951 |
3/15/2015 6:22 PM | |
Posts: 9 Rating:
|
ok..i understand. so what should be the HW config of CPU 313c-2dp look like. I have attached the pic. let me know if its correct. also i have attached network config. also the profibus connector settings at both ends are "ON". Do i need to set PG/PC interface in PC station as pc internal local or CP5622(profibus)?
AttachmentDesktop.rar (51 Downloads) |
3/15/2015 6:48 PM | |
Posts: 9 Rating:
|
i will give try and check now. the pg-pc setting is by default in pc internal local. |
Follow us on