4/29/2012 11:03 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Look in the system manual: http://support.automation.siemens.com/WW/view/en/36932465 Extract of the system manual about the DP Master module (p446): Other communications services of the CM 1243-5 The CM 1243-5 DP master module supports the following additional communications services: ● S7 communication – PUT/GET services The DP master functions as a client and server for queries from other S7 controllers or PCs via PROFIBUS. – PG/OP communication The PG functions allow the downloading of configuration data and user programs from a PG and the transfer of diagnostics data to a PG. Possible communications partners for OP communication are HMI panels, SIMATIC panel PCs with WinCC flexible or SCADA systems that support S7 communication. |
Best regards |
|
This contribution was helpful to
3 thankful Users |
Follow us on