5/11/2023 3:39 PM | |
Joined: 11/8/2017 Last visit: 7/12/2024 Posts: 328 Rating:
|
Hi, Yes, there is a ready-made block that will do exactly what you're looking for. The block name is TPHI_HX. See attached screen dumps. You can connect your dry bulb temperature and humidity inputs to the associated Input pins on the block (Input pins 'T' and 'HuRel'). You will also need to define the atmospheric pressure for your location (Input pin named 'AP'), and also set the 'EnTWet' input pin to Yes to allow the wet bulb calculation to work. The wet bulb temperature output pin is 'TWet'. You can access all the Help info for the block by left-clicking (highlighting) the block in CFC, and then press F1 on your keyboard. Regards, AttachmentCalcBlock.zip (440 Downloads) |
Last edited by: CJ. at: 05/11/2023 15:40:21 |
|
This contribution was helpful to
1 thankful Users |
Follow us on