11/25/2011 4:29 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello Nashwa Which PLC you are using ? There are two possibilities of transferring the S5 program to an EEPROM. 1. You can load the program in EEPROM using the EPROM programming port built into a SIEMENS PG. Or use a Siemens External EPROM programmer. 2. You can also download the program to S5 90U/95U/100U CPU using your cable and then copy it to the EEPROM. Pl see the manuals a) S5 90U 95U - See Section 4.4.1 http://support.automation.siemens.com/WW/view/en/1091648 b) S5 100U - see Section 4.4.1 http://support.automation.siemens.com/WW/view/en/1091978 Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
1/27/2015 10:53 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|
Follow us on