10/1/2011 10:30 AM | |
Joined: 1/28/2009 Last visit: 6/11/2024 Posts: 6841 Rating: (1359) |
Dear Milosh To do so, you have to assign a bit memory in the CPU's properties.In hardware configuration-->CPU properties-> cycle/clock memories-->clock memory.Enable the clock memory and define a memory byte number as you like.In PLCSIM,you should download the hardware with program .Check the STEP7 online manual for frequencies corresponding to each bit position in the memory byte. Best regards |
10/3/2011 10:08 AM | |
Joined: 8/16/2010 Last visit: 5/16/2024 Posts: 636 Rating: (12) |
I do that but it didn't work... Bit not changing... |
10/3/2011 10:15 AM | |
Joined: 1/28/2009 Last visit: 6/11/2024 Posts: 6841 Rating: (1359)
|
Dear Milosh Please give us the version of your STEP7 and the simulating module.If possible upload your test project. Best regards |
10/5/2011 11:55 AM | |
Joined: 8/16/2010 Last visit: 5/16/2024 Posts: 636 Rating: (12) |
THANKS A LOT. I finally got it to work. |
This contribution was helpful to3 thankful Users |
5/30/2014 3:52 PM | |
Joined: 5/30/2014 Last visit: 6/6/2024 Posts: 142 Rating: (17) |
Hi hdhosseini and Hristo, I did what hdhosseini advised Milosh in his post 10/1/2011. However, nothing happens in M0.5 . I connected that bit to one pin in CFC, but nothing happens again. My STEP7 version is 5.5.1.0 + SP1. CPU: 314C-2 PN/DP @hdhosseini: thanks for advice(s), I will use hint(s) too. Here is a sample project: AttachmentTest.zip (205 Downloads) |
Last edited by: C-3PO at: 5/30/2014 3:55 PMIf you find my contribution helpful please RATE it :)) |
|
5/30/2014 4:02 PM | |
Joined: 1/28/2009 Last visit: 6/11/2024 Posts: 6841 Rating: (1359)
|
I only downoaded the hardware to PLCSIM here via PROFIBUS.In PLCSIM it works perfectly.Your project also has an internal error.I did not check the whole codes but the clock merker works.
|
This contribution was helpful to1 thankful Users |
Follow us on