5/22/2006 12:46 PM | |
Joined: 10/10/2005 Last visit: 7/24/2024 Posts: 1917 Rating:
|
Hello, regarding to your inquiry we would like to inform you. Normely you will receive the area lenght error if you want to store a lenght of data example in a data block or in a marker byte/word but the area of the data block or marker byte is to short. Example you want to store a lenght of data with 0 up to 10 bytes in a data block. But the bigest address ofdata block is only DBB 5 (max. 5 bytes). So you have to expand the addresses/bytes of the data block. Please see the home page of the SIMATIC customer support and find the following FAQ which do you will find by the quoted Beitrags-ID: http://www.siemens.com/automation/csi_en/product Why does the area length error appear in the CPU's diagnostics buffer?Beitrags-ID: 23151678 With best regards Cicero |
Follow us on