5/24/2014 7:39 AM |
|
Posts: 235 Rating: (52) |
Dear All, What is the mjor defference between SIMOCOD PRO V/C and simple DOL/STAR DELTA protection of motor? or say what is the adavntage of SIMOCODE? |
5/26/2014 5:26 AM | |
Posts: 262 Rating: (45) |
Hi, Let me understand your question first... Do you want to know:- 1) What is difference between Simocode pro C and V? Well to answer this pls refer the litreture attached. In short... pro C is used for DOL and RDOL starting methods and provides current based monitoring and protection. ProV is used for everything which proC can do + for Star Delta applications too. It also provides Current as well as Voltage based protection. 2) Difference between Normal way of Star Delta Starting and Using Simocode? Normally Star Delta is used to reduce Starting current of any Sq Cage Ind Motors, this helps in reducing the stress on Stator windings also controlling the Voltage dip in the bus while starting big motors. Simocode used in such circuits helps in eliminating complex star delta wiring and also provides RUN feedback to the DCS. It also provides "n" no of protections to big motors like Phase failure/ reversal, earth fault, No of Hot/ Cold Starts, contactor welding etc which is either not avaibale in normal star-delta starter or you have to use seprate monitoring relay for it. My Suggestion... If you have to communicate motor paramters to DCS or you have to operate Motor feeders from Remote then only go for Simocode. This will save alot of control cabling and provides seamless integration with automation system. Else, you can use 3RB relays in normal Star-Delta Starters. AttachmentC:\Users\in210417\Desktop\01. SIMOCODE pro Brochure.pdf (290 Downloads) |
5/26/2014 7:03 AM | |
Joined: 5/12/2014 Last visit: 9/9/2020 Posts: 149 Rating: (16) |
Dear , Please refer thislinkfor the defference between SIMOCOD PRO V/C and simple DOL/STAR DELTA. |
5/26/2014 2:39 PM |
|
Posts: 235 Rating: (52) |
Dear Thanx to try for reply but i cant understand.can u explain in brief what u want to say???? |
Follow us on