11/28/2016 8:14 AM | |
Joined: 5/17/2010 Last visit: 5/22/2024 Posts: 226 Rating:
|
Hi, As written at the following FAQ: -"Remote" mode is active(device is exchanging data with PLC) If it is not possible to remedy the above causes, (...) you can upload, correct and save your actual parameterization and restore the factory defaults on the SIMOCODE pro device (see system manual chapter “Restoring the factory settings with the TEST / RESET button on the basic unit”) So maybe you can disconnect the PLC (brake the data exchange) and get direct access with your PC tp SIMOCODE to change the S1 (or S2) to get the option for local/remote switch. Else you have to go the way with restore factory settings.... With best regards Michael |
Last edited by: Mr. SIRIUS at: 11/28/2016 8:21:53 AM------------------------------------------------------------------------------------------------ |
|
Follow us on