2/17/2021 11:03 AM | |
Joined: 1/4/2007 Last visit: 7/11/2024 Posts: 1134 Rating: (175)
|
Hello Jiri, The parameter „ERROR_CODE“ is the data-/command-error code. E.g. when you send the DR3 to the WP321 and the Service mode is not on. If so, you receive a data-/command-error. The data-/command-errors are explained in the WP321 manual, into the chapter 9.5.3: https://support.industry.siemens.com/cs/ww/en/view/109770838 When you disconnect the cells, you have to check the bit: s_IO_DATA => SCALE_STATUS => ERROR Best regards Siwarexi |
Follow us on