11/24/2016 5:05 PM | |
Joined: 11/10/2016 Last visit: 4/17/2019 Posts: 2 Rating: (1) |
Hi there, I'm not sure if this is the right place to post this but the issue I'm facing is similar to AdasK initially but it then evolved into something else. In my PC, I had Step 7 OEM SP2 which I tried to install STARTER 4.5. After a successful installation, when I tried to start a new project, I got the message where it said "This application has encountered a problem and needs to close". I followed the suggestion in this forum to uninstall Step 7 and re-install STARTER. When I opened STARTER, I was greeted by the "Installation Error" message (see attached). After about 5 clicks the Project Wizard was showing. Then, when I tried to start a new project I got the attached message about "New user project (257:5)". I had to press "OK" for more than 5 times before it goes away. This can't be right, can it? When I check the installation, I have SIMATIC CFC V8.2 installed but some how it is not recognising it. Please can you help? My OS is Windows 7 Professional with the following Siemens software installed: SIMOCODE ES DIGSI 4.87 Thank you in advance for your help. Regards, Joon ------------------------------------------------------------------------------------------ AttachmentStarter error 2016 11 24.zip (379 Downloads) |
Last edited by: Min_Moderator at: 11/25/2016 12:58:07 PMNew subject after splitting |
|
Follow us on