2/16/2011 5:47 PM | |
Joined: 12/21/2009 Last visit: 7/3/2024 Posts: 39 Rating:
|
Hello! I don't recive any error message so I don't have any clue from Siemens. In Attachement You can find two folders. In one folder - V5.4 are screenshots from PC where is STEP V5.4 installed - as You can see everything is OK - I can see PROFINET nodes and assign names to them. On this computer I have also WinCC flexible 2007. In another folder - V5.5 are screenshots from PC where is STEP V5.5 installed - as You can see nothing is OK - I cannot see PROFINET nodes and I cannot assign names to them. On this computer I have also WinCC flexible 2008 SP2 installed. As You can see from screenshots OS is the same: Windows XP Proffesional SP3 I hope that You can find out where is the problem with this information. Thanks azi1984 AttachmentV5_5 V5_4.zip (348 Downloads) |
Follow us on