6/16/2011 3:21 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, The IM151‑8PN/DP CPU interface module can be used as a time client at the PROFINET interface by using the NTP method. At the PN interface, there is only the functionality as a time client. So, for that reason the other options there isn't active. Perhaps the this FAQ will helps you How do you configure a PC as NTP server?. You will need uncrossed twisted pair cable for connection. Best regards, Hristo MIhalev |
6/16/2011 5:38 PM | |
Joined: 7/29/2008 Last visit: 7/11/2024 Posts: 96 Rating: (4) |
It seems there is no way to set PLC time to Local with NTP. Every time that it is needed you have to calculate it through FC61 BT_LT /tf/WW/en/Posts/23381 FC61 BT_LT https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=19324378&objAction=csOpen&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW |
Follow us on