7/30/2024 7:06 AM | |
Joined: 2/26/2024 Last visit: 10/16/2024 Posts: 50 Rating: (0) |
Hi, I am trying to achieve a functionality on WinCC unified V17 that shows the heartbeat or an animated gif that shows/updates on the HMI every second to show that the PLC is communicating with the HMI. Let's say if the communication is good whatever the gif is - it should be green and red if not communicating. I'm looking for something as attached or even two circles in intersection and is constantly moving or flashing. I could not find an answer, and I'm unable to delete the prev post but I believe you commented it as it was posted twice. Please guide me. Thanks. AttachmentFiles.zip (416 Downloads) |
8/2/2024 9:04 AM | |
Joined: 7/30/2024 Last visit: 10/17/2024 Posts: 242 Rating: (5) |
Locked because posted twice. The active topic can be found here: Kind regards, Moderator_Lan |
Follow us on