8/28/2019 10:52 AM | |
Joined: 1/30/2019 Last visit: 10/15/2024 Posts: 54 Rating: (2) |
Hello, I have a WM with XWP 6.1.384 installed (also all updates), I have problems to download firmware and configuration of PXG3.L. Error in image01 appear when I try to download the firmware, Error in image02 appear when I try to download the configuration I tried with several PXG3.L but the error is always the same. I have no problem to download Ethernet PX like PXC22ED for examples. For now I solved using the old VM with XWP 6.1.242 just to configure the PXG3.L. I tried to install XWP 6.1.384 on a new VM but the result does not change. Settings of Antivirus, Firewall ecc are the same on both VMs. no one with the same problem?
AttachmentImage.zip (404 Downloads) |
9/1/2019 9:38 PM | |
Joined: 1/30/2019 Last visit: 10/15/2024 Posts: 54 Rating: (2) |
Ok, now it's working! Thks. |
Follow us on