7/20/2010 2:20 PM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
The MPI programming port dependency of PLCSIM has already been "fixed" with the releaseof PLCSIM V5.4 in late 2007 dear stevennoppe(what version are you using?). Current version is V5.4 SP3 andnow also allows running of multiple PLCSIM instances at the same time and (some forms of) PLC to PLC communications between them. I hope this helps |
Cheers |
|
7/20/2010 2:38 PM | |
Posts: 65 Rating:
|
I use V5.3 SP1. Time to buy the new version I guess or is the upgrade to V5.4 free? |
7/20/2010 2:50 PM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
I'm afraid not (Service Packs are free, but you will have to buy an upgrade from V5.3 to V5.4) |
Cheers |
|
7/20/2010 4:16 PM | |||
Joined: 9/27/2006 Last visit: 9/15/2025 Posts: 12408 Rating:
|
Herllo Steven; FYI, here is some upgrade information for PLCSim v. 5.4 SP3: http://support.automation.siemens.com/WW/view/en/36068835
Hope this helps, Daniel Chartier |
||
Follow us on