Default Header
(header konnte nicht geladen werden)
3/30/2008 5:22 PM | |
Joined: 2/22/2006 Last visit: 10/23/2014 Posts: 17 Rating: (2) |
Hello, please find attached a suitable tool for determing your requests. Please choose under the tab - Sensor your specific sensor: VS721 or VS721-A and - Lens: 35 (mm) - determine your maximum working distance e.g. 300mm => Hit the FOV-Button and the tool calculates an appropriate FOV (in this example ~ 43x32mm²) Please note that these "toolvalues" are only for orientation to choose an appropriate lens before buying the HW. You`ll receive the real values only with the real HW (Camera+Lens+Intermediate Ring)!!! Hope this helps?? Greetings AttachmentLensSelect_1.0_eng.zip (818 Downloads) |
Last edited by: MadMax at: 4/1/2008 6:09 PMLast edited by: MadMax at: 4/1/2008 6:08 PM |
|
Follow us on