12/28/2022 9:22 AM | |
Joined: 2/17/2020 Last visit: 5/13/2025 Posts: 2 Rating:
|
I currently have a little case with my IOT2050.. During upgrading debian's files with terminal commands probably i overwrote some image files. After succesfully upgraded and restart device, it's not able to boot system. Power lamp is pernament green, and stat lamp is red. I can read buffer by uart but it's not avaiable to break booting. In attachment log from putty. Based on the log, can we tell if it can be fixed without reinstalling the system? Otherwise, how can I abort the boot and change the boot priority when I can't buffer the request? Attachment20221228_forum_iot2050_txt2.txt (553 Downloads) |
1/2/2023 7:30 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, which command did you use to upgrade Debian? I suspect that it may have upgraded the kernel as well to 5.x, which is incompatible to the firmware you are using. With the Firmware V1.0.0 you can only use the Example Image V1.1.1 with Kernel 4.19. I would recommend to use the latest firmware and use Example Image V1.2.2. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on