11/13/2019 10:19 AM | |
Posts: 9 Rating:
|
A little update and another question. Thanks to your help I have succefully send some values (only 6 to test) to the LOGO! device using HMI recipe capability and I can also easly modify them using web server. The problem is I'm not sure if that's what I was looking for. Firstly, in the LOGO program I'm using six Network analog inputs (and there are only 32 of them overall, so not enougth even if I reduce those 96 values to 48) and six analog outputs. And the other problem is that I think I need those values to go one after another to the same output and change every 15 minutes. Is there some block that allows that? I've got only one AQ2 AM module and someone told by to use 4-20 current loop and PWM to connect it to the power regulator. Or is LOGO! wrong device for my project? Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/13/2019 11:43:16New subject after splitting |
|
11/13/2019 11:13 AM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35958 Rating:
|
Also use can use Parameter-VM-Mapping with a mathematical instruction instead of analog Inputs. |
Follow us on