9/26/2024 1:39 PM | |
Posts: 1 Rating:
|
Hi everyone, I am in the middle of a project in which I need to connect an edge device (catalogue attached) with SICAM A8000, CP-8021. The edge device will run on either windows 10 or 11 and will be running a Video analytics code written in Python. Is it possible for the edge device to communicate with CP-8021 and share outputs from the Python program using Modbus RTU protocol. Thanks, Kushagra AttachmentNuvo-9531 DATASHEET.pdf (647 Downloads) |
4/14/2025 9:40 AM | |
Joined: 4/14/2025 Last visit: 4/15/2025 Posts: 1 Rating:
|
Yeah, it's doable ust make sure your edge device supports serial ports or USB-to-RS485 adapters for Modbus RTU. Had to pause my Tele latino download last time I set that up! |
Last edited by: AutoGen_2757010 at: 04/15/2025 08:03:59 |
|
Follow us on