2/26/2018 2:49 PM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
I think, without password you have no change (see attachment).
AttachmentLOGO! Soft 0BA6 11_2009 page 219.pdf (291 Downloads) |
2/27/2018 5:10 PM | |
Posts: 53 Rating:
|
If the program is on the memory card, then you can copy it to the LOGO!. But note: Regards, |
2/28/2018 9:15 AM | |
Joined: 7/1/2014 Last visit: 5/7/2025 Posts: 237 Rating:
|
I saw this page but... The program is "Copy protected" -> yes So the copy never happen if I try to do it. We now have the password, but it allows me just to edit the program on the LOGO panel, and not to change the "Copy Protected" from yes to no. So it looks like the program can't be copied back on the LOGO if that option has been selected in the past and now is "trapped" in the memory card. If someone with a similar experience can confirm that...? From another page: https://support.industry.siemens.com/cs/ww/en/view/45164910/18270194315
|
Last edited by: dan.v. at: 2/28/2018 9:16:30 AMLast edited by: Jen_Moderator at: 2/28/2018 11:19:50 AMOptimized link. |
|
Follow us on