(0)| 9/16/2018 7:41 PM | |
|
Joined: 1/1/2017 Last visit: 10/30/2025 Posts: 343 Rating:
|
Hi Andrewz, As per the discussion if the Source File is not available in the backup or Uploaded Backup of PLC then is it sure that no modifications in logic can be made in the block? Actually I've been facing a problem in OB1.....The uploaded Backup has SCL script in OB1. I've added some logic in OB1 & also called a FC in OB1 in the STL & LAD language....Problem facing is that the Logic is getting downloaded but not going to Run mode.....RUn indication is coming but Running status is in Hold mode..... So if I've to find out the Source file where & how can I discover it and also how to regenarate the source file again! Regards OmKris ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/17/2018 8:28:58 AMNew subject after splitting |
|
| 9/17/2018 8:30 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject When going online the block is not showing running status & the logic is not working is published within the conference STEP 7 / STEP 7 Lite. Best regards, Jen_Moderator |
Follow us on