Default Header
(header konnte nicht geladen werden)
12/21/2009 10:33 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi Kankumo, you mean If you have created a Big function Block (or multiple instance)so you have to create manually DB for same? if it is you Question then no. it will created by the Software only. you have to just Declared in State & call, then just call the FB & give the DB no. Software generate the DB with all your declared variables. here is the Example http://support.automation.siemens.com/WW/view/en/18723826 |
Ammy |
|
Follow us on