10/9/2024 5:54 AM | |
Joined: 6/18/2022 Last visit: 9/11/2025 Posts: 15 Rating:
|
Hello, I have made some scripts that sum values (bacnet points from logical view) and write the result of the sum into a virtual analog of Desigo. This virtual analog is under trend. I have seen that the sum result never changes. (bacnet points increase constantly, they are electrical energies) The only way to make the script work correctly is to open the graphics pages where I put the points (so the sum is right) Why? Are the scripts dependent on the points in graphics? Did I make a mistake in editing the script? [An example is attached.] Thanks AttachmentScript.txt (270 Downloads) |
Last edited by: Moderator_Lan at: 10/09/2024 08:17:54Code attached |
|
10/10/2024 6:18 AM | |
Joined: 10/12/2023 Last visit: 9/15/2025 Posts: 120 Rating:
|
Hi. Firstly, I haven´t seen a brace for a close "while".
And graphics shouldn't matter here. Attachmenttest.txt (274 Downloads) |
Best regards, |
|
10/14/2024 5:31 AM | |
Joined: 10/12/2023 Last visit: 9/15/2025 Posts: 120 Rating:
|
Hi. Can you show the new script, just for information ? Have a good day! |
Best regards, |
|
10/14/2024 2:54 PM | |
Joined: 6/18/2022 Last visit: 9/11/2025 Posts: 15 Rating:
|
HI, |
Follow us on