12/26/2008 12:49 PM | |
Posts: 217 Rating:
|
Sorry i send the wrong link here is the correct one https://support.automation.siemens.com/WW/llisapi.dll/csfetch/23183356/STEP7_HSPs.zip?func=cslib.csFetch&nodeid=27079579 |
12/26/2008 1:53 PM | |
Joined: 6/10/2008 Last visit: 7/3/2025 Posts: 197 Rating:
|
Thank you, it went OK! |
12/27/2008 4:51 AM | |
Posts: 217 Rating:
|
You are welcome.
|
12/28/2008 6:26 AM | |
Posts: 107 Rating:
|
Hi, Arunakat1, My software for S7 also have this problem, need to HARDWARE UPDATE ( my existing Ver 5.03). Could you please help me to get this HARDWARE UPDATE in afile or compress file ? because my notebook can not connect to the internet. I hope you do not mind , sending the file HARDWARE UPDATE to my email address :indrasurya@gmail.com, i'd be grateful. Regards, INDRA |
12/28/2008 9:27 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Andra, If you look on this link, you could download the HSP. STEP 7 Hardware Support Packages (HSPs - Stand: 11/2008) Please consider that the first version of STEP7 that could use the HSP is STEP7 V5.2 If you have an older version then it is not possible to read in the HSP ! When you have a newer version then it is also not possible to read in all HSP's, when there is a need for a version to program the hardware then it is not possible, see also the pdf's that you can download from the same url. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on