Default Header
(header konnte nicht geladen werden)
4/28/2010 8:17 AM | |
Posts: 116 Rating:
|
Hi, see manual: http://support.automation.siemens.com/WW/view/en/27002365 Chapter 2.7 and 6.3 I think one limit might be the maximum permissible message frame lenght (depending on the bus system). Moreover the computing load of each TM17 must be considered equivalent to one half of a SINAMICS axis, which leads to a reduction in the number of axes on the part of drive control. Regards Kai |
4/28/2010 3:13 PM | |
Posts: 3 Rating:
|
Hello Christoph, It will be2 CU320's with the latest FW. Thanks for your feedback. |
4/28/2010 3:37 PM | |
Posts: 3 Rating:
|
Kai, Thanks for the infomation. It was very helpful and clarifies what I needed to know. Regards, Dave K. |
Follow us on