12/13/2011 10:07 AM | |
Posts: 140 Rating:
|
Actually I have done programming for the modules above, I wanted to get expert opinion of how to make my program robust. Any tips would be appreciated!
|
12/19/2011 1:12 AM | |
Posts: 140 Rating:
|
Hello Experts, I am writing many network Ladders for generating alarms based on some conditions, however i want to trigger alarm after some delay in case the alarm conditions are met. In the atatched program, I am using an ODT before each alarm trigger bit to turn On alarm after say 2s in case the alarm condition is met. My Question is, I have to generate 40 or more such alarms, so do I need to use seperate ODT timers before each Alarm trigerring bit? or is there any other way to avoid this. If there is, that i suppose will save processing power and time both. Please suggest accordingly! Thanks in advance! rgds, Syed AttachmentFC30_Alarm.pdf (483 Downloads) |
12/20/2011 7:41 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
Hi Well yes you can save on S5 timers if you use IEC timers, Have fun... |
Jazz |
|
Follow us on