Default Header
(header konnte nicht geladen werden)
1/1/2009 6:03 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Based on the type you specified (6es5921-1AA21), your S5 system seems to be a Simatic S5-130A/Kwith a CPU 921. The type you mention is SIMATIC S5 921 CPU FOR CC 130A,CC 130K If I am correct, you will need a special programing unit like PG631 to connect to the PLC. And an interface AS501. Look here http://support.automation.siemens.com/WW/view/en/188176 And here: http://support.automation.siemens.com/WW/view/en/188158 Look here how a PG 631 look like http://support.automation.siemens.com/WW/view/en/19696894 |
Best regards |
|
Follow us on