Default Header
(header konnte nicht geladen werden)
4/4/2012 8:49 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
only one block read-write, the rest read-only? How can you activate the protection level with a password in the HW Config for an S7 CPU? |
4/6/2012 8:14 AM | |
Joined: 8/31/2010 Last visit: 7/18/2025 Posts: 1525 Rating:
|
Thanks Hello ezepecker, Know-How protection is used to protect your program blocksin the engineering phase. If you wanna pass on your project to some one, then after applying Know-How portection, without knowing the right password, no one can view / edit it. Bind to Serial Number of Memory Card or CPU is applicable only to S7-1200. This binding will help you to ensure copy protection is done... (Assume, if the program is downloaded to a different CPU or different Memory Card, then your code will not work) For more details on this - refer Setting up and removing block copy protection What do you mean by automatically? |
Like it? Rate it! |
|
Follow us on