Default Header
(header konnte nicht geladen werden)
6/1/2012 7:43 AM | |
Joined: 12/16/2011 Last visit: 9/3/2025 Posts: 9 Rating:
|
and command and it will not start? M1.0 "FirstScan" => "PID_3Step_DB".RunModeByStartup ??? |
6/1/2012 8:29 AM | |
Joined: 6/26/2009 Last visit: 11/27/2024 Posts: 122 Rating:
|
Hi , the parameter you mentioned is related to the checkbox "enable running last mode after CPU restart " and is not directly related to the fact if your PID is working or not. With the little of information you give , I think you also have this problem. PID not responding 1214 FW2.2 / V11 SP2 upd2 Is this your problem to ? koenb |
6/15/2012 8:57 AM | |
Joined: 12/16/2011 Last visit: 9/3/2025 Posts: 9 Rating:
|
Another test after update 3 (for TIA): DB_PID is locked and when browsing the parameters can not find in the parameter "retain > Mode and therefore do not know how to set it to 3 see 3x screens in Attachment AttachmentStart_PID.zip (550 Downloads) |
Last edited by: O_Moderator at: 6/15/2012 10:22 AMfile converted to zip-file |
|
6/15/2012 11:04 AM | |
Posts: 267 Rating:
|
Hello, I think you try to set an Intger to a output (Bool). Please use the MOVE-function to set "Retain.Mode" to "3". |
Follow us on