4/25/2012 10:52 PM | |
Posts: 64 Rating:
|
I have a Step 7 test program with STL attached. This is a program for Set CPU clock from an external source (for ex. An OP Panel). I have some questions about it: 1- In network 5, there is a code saying “T LB 3”. What does LB3 means? As I know DBB15 refers to Byte 15 of DB51. But I cannot understand where LB3 is pointing to. 2- In network 6, what does it mean “PDT :=#TEMP3”?! As I know PDT is the Input variable of SFC0 (set Clock) that receives the time from external source. But TEMP3 is a temporary variable that has no value inside the block. So which value is assign to the PDT of SFC0? Sincerely Mazdak AttachmentSTL_Test_Program.zip (108 Downloads) |
Last edited by: mazdak at: 4/25/2012 10:53 PM |
|
4/25/2012 11:39 PM | |
Posts: 1064 Rating:
|
take a look at this it should answer your questions http://support.automation.siemens.com/WW/view/en/22819915 |
Follow us on