1/28/2025 6:38 AM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hi stu_mcleod145, The licensing of WinCC Unified PC Runtime is based on the number of PowerTags required. I have not yet used a test license for WinCC Unified PC Runtime, but your message says that it only covers 500 PowerTags. If you use the context menu for your panel within the project tree and select 'Properties…', you will find the number of PowerTags used under 'General > Information'. The license warning does not affect the functionality of the system. I assume you are using a real PLC (not a simulation) and therefore you need to configure your interface to make communication work. Please have a look at the FAQ 'Setting the PG/PC interface for WinCC communication with the controller'. Please also make sure that your PLC is configured with the correct date and time. This is important because the communication is secured by using certificates that have a validity period. TIA Portal is a very comprehensive software framework. Probably one of the most comprehensive software projects done in Visual Studio. Although the development does a lot to improve the performance, the software has high requirements and still not a real sufficient performance. Kind regards
|
This contribution was helpful to
1 thankful Users |
1/28/2025 2:57 PM | |
Joined: 7/19/2022 Last visit: 9/11/2025 Posts: 436 Rating:
|
Hello stu_mcleod145, First of all, please note that the license you see "WinCC Unified PC RT - V17.0 (missing number: 163)" refers to a license independent of the TIA Portal V17 trial. If you do not want this window to appear, you must purchase this license, although if you are only going to simulate, you can close the message and that's it. Even so, this should not be the problem for not communicating. According to what you attached, it seems that the HMI connection is correct. Check in the properties of the S7-1200 that the box "Only allow secure PG/PC and HMI communication" is unchecked. This box is under "Protection & Security > Connection mechanisms" and as of TIA Portal V17 and S7-1200 with firmware ≥ V4 it is no longer necessary because the secure connection is implemented automatically. As for TIA Portal being slow, I don't really know what to tell you, but I am attaching the software and hardware requirements required: General software and hardware requirements |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
2/1/2025 9:09 AM | |
Joined: 1/19/2025 Last visit: 3/21/2025 Posts: 7 Rating:
|
Stephan - THANKS for the tip regarding Certificates. In the end , it would seem i had everything correct part from Windows Certifictes that would be acceoted in the Unified RT. I could not find in the end how to add the certificate that allowed Local Host to be accepted . I created a brand new project , 3 tags in PLC , 3 in HMI , and still the project would throw the aspect of a Not Trusted website ( 127.0.0.1 ) be an Insecure website etc . The ONLY thing that worked in my case was to fully uninstall all of TIA Portal & Simulation , reinstall , and this time i was prompted with a page that created a Certicate , of which I said YES PLEASE !! Immediately my projects that i had created in Trial were wunning correctly on Simulation in PLC and HMI with Unified RT . I was hoping it was the Time and Date - that was not an easy thing to find either , but the certificate generation was the problem. Thankyou again. Cheers Stu |
Last edited by: Moderator_Lan at: 02/03/2025 08:27:37Text formatting optimized |
|
This contribution was helpful to
2 thankful Users |
Follow us on